{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Replacement for obsolete S48890 RIM module for ZSI
Issue:
What is the replacement for the obsolete RIM module S48890?

Product Line:
Circuit Breakers

Environment:
RIM and ZSI Interface

Resolution:
The replacement for the RIM in ZSI applications is LV848892SP.  This module also works with the Masterpact MTZ
See attached for instructions.

Note: LV848892SP will not work for AMS applications.  For AMS applications it will be necessary to convert to the ERMS arc-flash incident Energy Reduction Maintenance System.

Schneider Electric Canada

Attachment(s)
LV848892SP ZSI Interface NHA12883.pdf [3.68 MB]
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.