{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What are the dimensions of the handle and shaft on the GV2AP01 and GV2AP02 external operator kit?
Issue:
Identify the dimensions for the handle and shaft kit for GV2AP01 and GV2AP02

Product Line:
Manual Motor Starters, Controllers, and Protectors

Environment:
GV Manual Motor Starters

Resolution:
The handle height and length are both 65 mm, thickness is 53 mm.The shaft diameter is 7 mm. See attached drawing for complete dimension and door cut-out guide.

Schneider Electric Canada

Attachment(s)
GV2AP01 Dimension.pdf [71.31 KB]