{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What are the LED indicators mean on ION9000, and where are they located?
Issue
The user would like to know the LED indications on ION9000 Display.

Product line
ION9000

Environment
ION9000 Display

Cause
End user would like to know what the LED indicators mean on the ION9000 and where they are located

Resolution
The following picture shows the Status and Alarm LED on the Display.

Status and Alarm LED

The following table provides descriptive information about the Status and Alarm LEDs.​

Status and Alarm LEDs Table


Schneider Electric Canada