Issue:
Can you get an Actuator and Zone valve assembled ?
Product Line:
Valves and Actuators
Environment:
Ordering
Cause:
Procurement
Resolution:
CV information recommended but an example for the Steam rated Valves would be:
1/2" = VS2213G14A020
3/4" = VS2313G14A020
1 1/4" = VS2517G14A020
Steam rated valves "VS" are needed for the High temperature rated AG14A020 actuator , "VT" valves would be for general On/Off valves and AG13A020 actuator .
Can you get an Actuator and Zone valve assembled ?
Product Line:
Valves and Actuators
Environment:
Ordering
Cause:
Procurement
Resolution:
CV information recommended but an example for the Steam rated Valves would be:
1/2" = VS2213G14A020
3/4" = VS2313G14A020
1 1/4" = VS2517G14A020
Steam rated valves "VS" are needed for the High temperature rated AG14A020 actuator , "VT" valves would be for general On/Off valves and AG13A020 actuator .