Search FAQs
What are the warranty options for PowerLogic and ION monitoring and control products?
Product Line
PowerLogic and ION Monitoring and Control Products
Environment
Warranty
Cause
A customer may require information about the standard warranty and additional extended warranty options for PowerLogic and ION products.
Resolution
PowerLogic and ION Monitoring and Control Products
Environment
Warranty
Cause
A customer may require information about the standard warranty and additional extended warranty options for PowerLogic and ION products.
Resolution
Warranty Options Available | ||||
Product Range | Standard Warranty (Months) | Option 1 | Option 2 | Option 3 |
Energy, Power, and Power Quality Meters | ||||
ION8650 Series | 120 | |||
ION7400 Series | 60 | X | X | |
ION9000 Series | 60 | X | X | |
PM5000 Series | 60 | X | X | |
PM8000 Series | 60 | X | X | |
3020 Series | 18 | X | ||
BCPM Series | 18 | X | ||
CM4000T Series | 18 | X | ||
EM3500 Series | 18 | X | ||
EM4000/EM4800 Series | 18 | X | ||
EM4200 Series | 18 | X | ||
EM4300 Series | 18 | X | ||
EM4800 Series | 18 | X | ||
EM4900 Series | 18 | X | ||
EMB/EME Series | 18 | X | ||
ION6200 Series | 18 | X | ||
ION7550/ION7650 Series | 18 | X | ||
PM3200 Series | 18 | X | ||
iEM3000 Series | 18 | X | ||
Energy Servers and Gateways | ||||
EGX Series | 18 | X | ||
Com'X Series | 18 | X |
The warranty starts from the date of invoice of the products.
Standard Warranty: The duration of the standard warranty is specified in the table contained in this document.
Option 1 – Extended: 2 to 5 years from Shipment.
Option 2 – Extended: 6 to 10 years from Shipment.
Option 3 – Premium support: 10 years from Shipment.
Please see the attached document for more detailed information on the Standard Warranty and Extended Warranty Options.
Released for:Schneider Electric Canada
Attachment(s)
Explore more
Range:
Explore more
Range: