{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Do the BMENOC0301 and BMEH58x040 modules need to reside on the same network?
Issue
When adding NOC modules, must they fit into the CPU network configuration parameters?

Product line
Modicon M580

Resolution
No. You can add a BMENOC0301 in each local backplane and give it an IP address on its own network. Leave the backplane port deactivated in this configuration.

Schneider Electric Canada