Issue:
How to close a PowerPact RG, RJ, RK, or RL circuit breaker
Product Line:
Molded Case Circuit Breakers
Resolution:
When the PowerPact R Frame breaker trips, the handle moves to a center TRIPPED position. To close the breaker, it first must be reset, which means the handle must be moved from TRIPPED to the OFF position. Because internal springs are being compressed when this is done, some force will be needed. Once the breaker has been reset, the breaker can now be closed by moving the handle to the ON position.
How to close a PowerPact RG, RJ, RK, or RL circuit breaker
Product Line:
Molded Case Circuit Breakers
Resolution:
When the PowerPact R Frame breaker trips, the handle moves to a center TRIPPED position. To close the breaker, it first must be reset, which means the handle must be moved from TRIPPED to the OFF position. Because internal springs are being compressed when this is done, some force will be needed. Once the breaker has been reset, the breaker can now be closed by moving the handle to the ON position.
Released for:Schneider Electric Canada