Search FAQs
What is a Class 1 Div 2 Actuator for a VB-7313-0-4-11 2" 3W Mixing valve with 24VAC power and 0-10VDC Control signal?
Issue:
Is there a Class 1 DIV II actuator available for the VB-73XX 3 way mixing valve ?
Product Line:
Valves and Actuators
Environment:
Application
Cause:
Product Features
Resolution:
The MP6-361 Actuator can be used , but a CP-9301-456 Drive with 0-10VDC, will need to be remote mounted out of hazardous area .
The Linkage kit AV-29 is going obsolete when stock is depleted .
Is there a Class 1 DIV II actuator available for the VB-73XX 3 way mixing valve ?
Product Line:
Valves and Actuators
Environment:
Application
Cause:
Product Features
Resolution:
The MP6-361 Actuator can be used , but a CP-9301-456 Drive with 0-10VDC, will need to be remote mounted out of hazardous area .
The Linkage kit AV-29 is going obsolete when stock is depleted .
Released for:Schneider Electric Canada
Explore more
Range:
Explore more
Range: