Search FAQs
How to write to ClearSCADA DataTable from Excel using VBScript and ODBC
DISCLAIMER
The example below is intended to demonstrate one or more features or methods and is presented as a configuration example only. Schneider Electric assumes no liability for the use or application of this example or any portion thereof.
Sometimes it is helpful to be able to write to a ClearSCADA DataTable from an external tool.
As an example, the following code, written in VBScript inside an Excel spreadsheet, will add a row in a DataTable called "Populate", which contains two fields, one string and one long value, as long as the DSN and credentials are correct:
Sub test()
Set ado = CreateObject("ADODB.Connection")
ado.Open "DSN=ClearSCADA", "Eng", "password"
If ado.State = 1 Then
MsgBox "Connected"
End If
queryText = "insert into Populate (Comment, Num) values ('AnyStringAny', 100)"
ado.Execute queryText
ado.Close
Set ado = Nothing
MsgBox "Done"
End Sub
The example below is intended to demonstrate one or more features or methods and is presented as a configuration example only. Schneider Electric assumes no liability for the use or application of this example or any portion thereof.
Sometimes it is helpful to be able to write to a ClearSCADA DataTable from an external tool.
As an example, the following code, written in VBScript inside an Excel spreadsheet, will add a row in a DataTable called "Populate", which contains two fields, one string and one long value, as long as the DSN and credentials are correct:
Sub test()
Set ado = CreateObject("ADODB.Connection")
ado.Open "DSN=ClearSCADA", "Eng", "password"
If ado.State = 1 Then
MsgBox "Connected"
End If
queryText = "insert into Populate (Comment, Num) values ('AnyStringAny', 100)"
ado.Execute queryText
ado.Close
Set ado = Nothing
MsgBox "Done"
End Sub
Released for:Schneider Electric Canada
Explore more
Range:
Explore more
Range: