What does error code 128 mean for the Unity Pro SCALING block?
Error 128 in the scaling block means that the IN_MIN and IN_MAX are not set. They can not equal each other. Call up an animation table and set them up in the CPU using the variable assigned to the PARA pin.
Released for:Schneider Electric Canada
Explore more
Range:
EcoStruxure Control Expert (Unity Pro)
Articles that might be helpful
Show more articles
Discuss this topic with experts
Visit our Community for first-hand insights from experts and peers on this topic and more.