{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What does the APPL light on the Quantum NOE indicate?
Issue
The 140NOE771xx module is displaying the APPL indicator. What is it and how is it cleared?

Product Line
Quantum

Resolution
The APPL indicator is simply letting the user know that there are entries in the NOE crash log. In order to view the contents of the log and reset the indicator a browser such as Internet Explorer, Firefox, Chrome, etc. can be used.  Enter the IP address of the NOE into the browser and navigate the NOE webpage. The default username = USER and the default password = USER.

Schneider Electric Canada