{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

What type of busbar plating used on the I-line Busway?

Issue:
Type of material coating the busbars on I-line II busway?

Product Line:
I-line and I-Line II Busway

Environment:
Products sold in North America

Resolution:
Bus bars for I-Line and I-Line II busway are plated to ensure low surface-to-surface contact resistance and to minimize surface corrosion.

Aluminum bus bars are electroplated with a coat of tin after preparation with the ALSTAN 80 process.
Copper bus bars are plated with a layer of silver that is flashed onto the surface of the bus bars.

Refer to page 15 of the 5600CT9101 2018 catalog. The link is provided below:
https://www.se.com/us/en/download/document/5600CT9101/

Schneider Electric Canada

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: