{}

Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
How can we help you today?
Can the Unity Quantum Hot Standby IO Scanner be altered online?
Issue
The IO Scanner in the Hot Standby system needs to be changed without interrupting the process.
Product line
Unity, Quantum, NOE, NOC
Resolution
Changing the IO Scanner constitutes a configuration change. Configuration changes are not supported between the Primary and Standby controllers and therefore must be done offline and the Quantum Hot Standby can not resync after an offline build changes. 

Upgrading from Quantum to M580 Hot Standby would make editing the IO Scanner possible in a bumpless manner as long as it can be accomplished by an offline build change. 

Schneider Electric Canada

Your browser is out of date and has known security issues.

It also may not display all features of this website or other websites.

Please upgrade your browser to access all of the features of this website.

Latest version for Google Chrome, Mozilla Firefox or Microsoft Edgeis recommended for optimal functionality.