Issue:
Applications requiring Class 1 Div 2 float switches
Product Line:
Float Switches
Environment:
NEMA Float Switches
Resolution:
The NEMA Type 7 and 9, class 9036, 9037 and 9038 switches are suitable for use on explosion proof applications. Suitable for Class I, Division 1 and 2, Groups C and D and Class II, Division 1 and 2, Groups E, F, and G hazardous locations.
Applications requiring Class 1 Div 2 float switches
Product Line:
Float Switches
Environment:
NEMA Float Switches
Resolution:
The NEMA Type 7 and 9, class 9036, 9037 and 9038 switches are suitable for use on explosion proof applications. Suitable for Class I, Division 1 and 2, Groups C and D and Class II, Division 1 and 2, Groups E, F, and G hazardous locations.