{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
iEM3000 Series Demand Capabilities
Issue
To read Peak Demand values from the meter

Product Line
iEM3455
iEM3465
iEM3555
iEM3565

Cause
The newer iEM34xx and iEM35xx meters provide demand values

Resolution

Demand readings are available in the iEM34xx and iEM35xx models from the below firmware versions. iEM34xx and iEM35xx models with older firmware versions cannot be upgraded.
  1. iEM34x5 - V1.2.003 and higher
  2. iEM35x5 - V1.1.001 and higher
  3. iEM3465 and iEM3565 - BACnet V2.4 and higher
CharacteristicsDescription
Peak Demand Values (iEM3455, iEM3465, iEM3555, iEM3565)
CurrentPer phase, neutral, and average
Active, reactive, apparent powerTotal

In a nonvolatile memory, the power meter maintains a maximum operating demand value called peak demand. The peak is the highest value (absolute value) for each of these readings since the last reset.

For information on how to set up, reset or read demand values from meter registers, please refer to attached iEM3000 User Manual.

Schneider Electric Canada

Attachment(s)
iEM3000 User Manual August 2017 - DOCA0005EN-08 (002).pdf [4.1 MB]