undefined [object Object]
{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What is the difference between a MS61-7203 actuator and MS61-7203-50 actuator?
Issue:
Can the MS61-7203-50 actuator be converted for 4-20mA ?

Product Line:
Valves and Actuators

Environment:
Application

Cause:
Product Features

Resolution:
The MS61-7203 Actuator has proportional input features for 2-10VDC and 4-20mA. The MS61-7203-50 Actuator has only 0-10VDC input option.
Also, the MS61-7203-50 Actuator cannot be field modified for 4-20mA. If using MS61-7203-50 actuator for 2-10VDC input, like the MS61-7203 actuator offers, movement will not be seen until at least 2 VDC using MS61-7203-50 actuator 0-10VDC system control .

Schneider Electric Canada