Issue:
Do single throw and double throw safety switch perform the same function?
Product Line:
Safety Switches
Resolution:
Single throw and double throw safety switches are used for different applications.

Do single throw and double throw safety switch perform the same function?
Product Line:
Safety Switches
Resolution:
Single throw and double throw safety switches are used for different applications.
- Single throw safety switches are used when the load is fed by only 1 source (such as normal utility power).
- Double throw safety switches are used when the load is fed by either of 2 sources (such as utility power or generator power), but not both at the same time. The transfer from one source to the other is manual (not automatic).
Released for:Schneider Electric Canada
Issue:
Do single throw and double throw safety switch perform the same function?
Product Line:
Safety Switches
Resolution:
Single throw and double throw safety switches are used for different applications.

Do single throw and double throw safety switch perform the same function?
Product Line:
Safety Switches
Resolution:
Single throw and double throw safety switches are used for different applications.
- Single throw safety switches are used when the load is fed by only 1 source (such as normal utility power).
- Double throw safety switches are used when the load is fed by either of 2 sources (such as utility power or generator power), but not both at the same time. The transfer from one source to the other is manual (not automatic).
Released for:Schneider Electric Canada