{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What Are the Auxiliary Contact Part Numbers for the GS Switches
Issue:
Auxiliary contacts for current GS1 and GS2 Fusible Disconnect Switches

Product Line:
Operating Mechanisms and Disconnect Switches

Environment:
GS2 Fusible Disconnect Switches

Resolution:
Part numbers for the auxiliary contacts are listed on the table below. See attachments for the instruction sheet.

Note:
GS1DU3 allows up to 2 auxiliary contacts and GS1DDU3 up to 4 auxiliary contacts without adding contact holder GS1AD10. For more auxiliary contacts, GS1AD10 is required.

Switch Amperes

Catalog No.

Description

30–800

GS1AM110

Auxiliary Contact, 1 N.O.

30–800

GS1AM101

Auxiliary Contact, 1 N.C.

30

GS1AD10

Auxiliary Contact Holder

Schneider Electric Canada

Attachment(s)
520332_01A55.pdf [5.5 MB]
30072-454-15_01.pdf [887.87 KB]