{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Is an Erie zone valve 0767C0036GA01 cross to a VT3343G13A02A zone valve?
Issue:
What is the replacement for a 0767C0036GA01 zone valve?

Product Line:
Valves and Actuators

Environment:
Maintenance

Cause:
Replacement

Resolution:
The 0767C0036GA01 part number crosses to a 2 Way 3/4" VT2343G13A02A assy , not a 3 Way VT3343G13A02A zone valve assembly.
Also, the 2 Way VT2343G13A02A with inverted Flare connection, is ONLY available in 3/4"

Schneider Electric Canada