Issue:
Do we have a substitute for the obsolete LU9AP12 rotary handle kit?
Product line:
Tesys U Starters
Resolution:
The GVAPR54 is the replacement handle, but they are not the same, so it will not work with existing. The piece on the end of the shaft is different. The GVAPR54 is the new handle that works with the LU9APN22 kit. You will need to replace the complete kit. See attached.
Do we have a substitute for the obsolete LU9AP12 rotary handle kit?
Product line:
Tesys U Starters
Resolution:
The GVAPR54 is the replacement handle, but they are not the same, so it will not work with existing. The piece on the end of the shaft is different. The GVAPR54 is the new handle that works with the LU9APN22 kit. You will need to replace the complete kit. See attached.
Released for:Schneider Electric Canada
Issue:
Do we have a substitute for the obsolete LU9AP12 rotary handle kit?
Product line:
Tesys U Starters
Resolution:
The GVAPR54 is the replacement handle, but they are not the same, so it will not work with existing. The piece on the end of the shaft is different. The GVAPR54 is the new handle that works with the LU9APN22 kit. You will need to replace the complete kit. See attached.
Do we have a substitute for the obsolete LU9AP12 rotary handle kit?
Product line:
Tesys U Starters
Resolution:
The GVAPR54 is the replacement handle, but they are not the same, so it will not work with existing. The piece on the end of the shaft is different. The GVAPR54 is the new handle that works with the LU9APN22 kit. You will need to replace the complete kit. See attached.
Released for:Schneider Electric Canada