{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What is the largest frame breaker that can be installed into an SBAD800?
Issue:
What is the maximum ampere rated breaker that can be installed in a SBAD800 (R) or SBSAD800 (R)?

Product Line:
Speed D board

Environment:
SBAD800, SBAD800R, SBSAD800, SBSAD800R

Resolution:
The largest ampere rating is 800A. The largest frame size is the Powerpact P frame at 800A. It is up to the specifier to make sure they do not exceed the total 800A rating of the distribution section and the upstream protective device. Please see the attachment for dimensions and specifications.

Schneider Electric Canada

Attachment(s)
SBAD800 SBSA800 SPEED-D09.pdf [68.58 KB]