{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Compact NSJ and Powerpact D frame motor circuit protector trip curves
Issue:
Trip curve estimate for Obsolete Compact NSJ  MCP and Powerpact D frame MCP

Product Line:
Circuit Breakers

Environment:
Motor Circuit Protectors:  Compact NSJ and Powerpact D frame

Resolution:
This product is Obsolete and there are no official published trip curves.  However, based on a UL and IEC literature review the attached power point presentation is the best estimate and should be used for reference only.  If official numbers are needed for arc flash studies etc.  then this product should be replaced with a newer product that has official documentation.

Schneider Electric Canada

Attachment(s)
Compact NSJ MCP Powerpact D MCP trip curve Estimate.pdf [369.38 KB]
Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: