Search FAQs
What are the recommended CT part numbers for the iEM3000 series meters?
Product Line
iEM3000 series meter
Environment
Current connection with iEM3000 series meter
Cause
In addition to using the part number guide to select the correct meter, CTs are required for the application
Resolution
Refer to the table for the recommended CT for the iEM3000 series meter:
Note: Only for iEM32xx used with 5A CTs
iEM3000 series meter
Environment
Current connection with iEM3000 series meter
Cause
In addition to using the part number guide to select the correct meter, CTs are required for the application
Resolution
Refer to the table for the recommended CT for the iEM3000 series meter:
iEM3000 series meter | Recommended CT |
iEM31xx | 63A Direct with Class 1 Accuracy |
iEM32xx | 1A or 5A CT with Class 0.5S Accuracy |
iEM33xx | 125A Direct with Class 1 Accuracy |
iEM34xx | 0.333V or 1.0V LVCT with Class 0.5S Accuracy |
iEM35xx | Rogowski coil (Rope CT) with Class 0.5S Accuracy |
Released for:Schneider Electric Canada
Explore more
Range:
Explore more
Range: