{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Will Wiser Energy work with my solar panels?
Most likely! Your incoming solar feed can connect directly into your main electrical panel, either through a breaker or a service-side tap.

If solar is set up in a subpanel, the incoming solar feed should be within 46" of the main panel as this will allow the provided current sensor cable to reach and connect to the Wiser Energy monitor in the main electrical panel.

If it is further than 46" extension cables are available in lengths of;
Length(Feet)Part Number
4'WISEREMCTEXT4
12'WISEREMCTEXT12
25'WISEREMCTEXT25
40'WISEREMCTEXT40

These extensions can be combined to achieve larger lengths, but the maximum length can be no more than 300'.

Wiser Energy

Schneider Electric Canada

Explore more
Product:
Range:
Articles that might be helpful Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product:
Range: