{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What certifications does Wiser Energy have?

In addition to extensive in-house testing, the Wiser Energy monitor has been tested to UL and IEC standards for safety, and certified by ETL/Intertek as safe to install in your home. Intertek is a Nationally Recognized Testing Laboratory (NRTL) and the ETL mark is functionally equivalent to the UL mark.

Wiser Energy, when properly installed, also meets all requirements laid out in the 2017 National Electrical Code (NEC). This means the Wiser Energy Monitor has been through an extensive set of industry standard safety tests to ensure that it is safe to use when plugged into electrical power and safe to use inside an electrical panel.

Per section 312.8, the Wiser Energy monitor and its current transformers are listed as a system, designed for field installation in a switch enclosure.

Wiser Energy also meets FCC Class B standards for electromagnetic interference.

All electrical devices emit electrical “noise” (in fact, the electrical noise emitted by the devices in your home is one of the things Wiser Energy uses to identify them!) — and the FCC has a strict set of limits and requires extensive testing to make sure they are not exceeded.

Wiser Energy has passed those tests and should not cause interference with other devices in your home.

  • Certified to CSA STD C22.2 No. 61010-1
  • Conforms to UL STD 61010-1
  • Conforms to UL STD 61010-2-032
  • Conforms to CAN ICES-3(B)/NMB-3(B)
  • Conforms to CISPR 32
  • Conforms to CISPR 35
Wiser Energy

Schneider Electric Canada

Explore more
Product:
Range:
Articles that might be helpful Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product:
Range: