The Wiser Energy monitor is intended to be installed inside new or existing Type 1 (Indoor) or Type 3R (Outdoor) 240V/120V Split-phase electrical panels.
The monitor itself is IPx0 rated and should be kept in a temperature range between 32°F (0°C) and 122°F (50°C).
Wiser Energy
The monitor itself is IPx0 rated and should be kept in a temperature range between 32°F (0°C) and 122°F (50°C).
Wiser Energy
Released for:Schneider Electric Canada