Issue:
Is there a replacement Actuator for a VAT-100-A65 Actuator?
Product Line:
Valves and Actuators
Environment:
Maintenance
Cause:
Replacement
Resolution:
The Valve and actuator will need to be replaced. If the existing valve is a 2 Way, use the p/n VB-7213-0-4-10 for the new valve. If the valve is a 3 Way, use the p/n VB7313-0-4-10 for the new valve.
The actuator VAT-100A65 crosses to a MF41-6083 floating actuator ,when used with a 1 1/2" valves. The Actuator will need the AV-611 linkage kit for mounting to the valve .
Is there a replacement Actuator for a VAT-100-A65 Actuator?
Product Line:
Valves and Actuators
Environment:
Maintenance
Cause:
Replacement
Resolution:
The Valve and actuator will need to be replaced. If the existing valve is a 2 Way, use the p/n VB-7213-0-4-10 for the new valve. If the valve is a 3 Way, use the p/n VB7313-0-4-10 for the new valve.
The actuator VAT-100A65 crosses to a MF41-6083 floating actuator ,when used with a 1 1/2" valves. The Actuator will need the AV-611 linkage kit for mounting to the valve .