{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Can the Micrologic X control unit on the Masterpact MTZ breaker be upgraded or replaced?
Issue:
Are the Micrologic 2.0X, 3.0X, 5.0X, 6.0X, and 7.0X control units replaceable and/or upgradeable on the Masterpact MTZ circuit breakers?

Product Line:
Micrologic Control Units

Resolution:
The control units are replaceable by Schneider Electric Services only. Services training is ongoing, therefore only some of the FSRs are qualified to perform the replacement. Check with Services for availability.

Standard control units commercial reference
UL
MicroLogic 3.0 X LV848815
MicroLogic 5.0 X LV847609
MicroLogic 6.0 X LV847608

IEC
MicroLogic 2.0 X LV847600
MicroLogic 5.0 X LV847602
MicroLogic 6.0 X LV847603
MicroLogic 7.0 X LV847604

NOTE: The commercial reference is printed on the front face of the MicroLogic X control unit. It also identifies the standard, IEC, or UL.

Schneider Electric Canada