{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Can a MS40-7170 actuator be used with shafts larger than 1/2" ?
Issue:
What can be used to adapt a MS40-7170 Actuator with a 3/4" Damper shaft?

Product Line:
Valves and Actuators

Environment:
Application

Cause:
Installation

Resolution:
The Optional Universal Mounting clamp for  5/8", 3/4" and 1" shaft sizes, use the AM-7563 Universal Mounting Clamp. see attached bulletin for Instructions

Schneider Electric Canada

Attachment(s)
MS40-7170 F-26748.pdf [590.03 KB]