{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Can Motor operators for H frame breakers (S29433) be installed in an I Line HCJ, HCP , HCRU Panelboards with a trim and door feature?
Issue:
Will motor operators fit into the Nema 1 and Nema 3R enclosed HCM Main lug only, I Line panelboard ?

Product Line:
I Line Panelboards

Environment:
Application

Cause:
I Line panel trim with door

Resolution:
The Nema 1, 4 piece trims without the door for HCJ , HCP, HCRU I line interiors, will allow the Motor Operator feature for the H and J Frame breakers to be installed.
The Nema 1, 4 piece trims with a door feature, will NOT allow the use of a motorized operator option.

Schneider Electric Canada