{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

What is the difference in C60SP, C60BP, and C60BPR Multi-9 devices?

Issue:
What is a C60?

Product Line:
Circuit Breakers

Resolution:
The following is a summary of the differences in C60SP, C60BP and C60BPR Multi-9 devices.

C60SP
C60SP devices are supplementary protectors as defined by UL1077 and CSA C22.2 No. 235.
They are for use within an OEM product such as a control panel and are not for use as branch protection (see attached for complete details).

C60BP and C60BPR
C60BP and C60BPR devices are circuit breakers, as defined by UL489 and CSA C22.2 No. 5.
They are for use as branch circuit protection and can also be used within an OEM product such as a control panel (see attached for complete details).
NOTE: The C60BP has factory installed mechanical lugs on each end. The C60BPR has factory installed ring tongue terminals on each end.

Schneider Electric Canada

Attachment(s)

0860CT0201 pp 9-13.pdf0860CT0201 pp 9-13.pdf [82.71 KB]
Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: