{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What's the difference between an AG13 / AH13 and AG14 / AH14 actuators ?
Issue:
What are the temperature rating differences bewtween AG13/AH13 and AG14/AH14 actuators?

Product Line:
Valves and Actuators

Environment:
Application

Cause:
Product features

Resolution:
The AG13 and AH13 are standard temperature (32-200 DEG F with 104 DEG F Ambient) rated , whereas the AG14 and AH14 actuators have a higher temperature rating of 32-250 DEG F with a 169 DEG F ambient rating .
The AG actuator is standard close off  and the AH actuator has higher close off.

Schneider Electric Canada