{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Video: How do you install and use the HOMELEC1PA padlock attachment to lock 1p, HOM, electronic breakers in the ON or OFF position?
Issue:
Instructions and video on how to install and use the HOMELEC1PA to lock 1p HOM electronic breakers in the ON or OFF position

Product Line:
HOM Breakers

Resolution:
Remove the trim (if installed) of the panel. Place the padlock device onto the face of the breaker, and use a screwdriver to bend the tabs on the device into the slots on the ON and OFF ends of the breaker. To padlock the breaker, move the handle to the desired position, and slide the padlock through the bail. The shackle of the padlock will prevent the handle from turning the breaker ON or OFF. For more information, see the video below or the attached instruction bulletin.

Schneider Electric Canada

Attachment(s)
HOMELEC1PA.pdf [973.59 KB]