{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Is there a blank module for the x80 I/O
Issue:
Does the x80 I/O have a filler module.

Product Line:
x80, M340, M580

Resolution:
We don't offer an x80 filler (empty) module but we do offer a cover which can be placed over the backplane connector. Its part number is BMXXEM010 and there are 5 covers included in the package.


Schneider Electric Canada