{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What is the rebuld kit for the VB-9213-0-5-13 valve?
Issue:
Is there a packing kit available for the VB-9213 valves?

Product Line:
Valves and Actuators

Environment:
Maintenance

Cause:
Replacement

Resolution:
The packing and cartridge assy only is p/n YBA-652-2. The total rebuild kit with stem that includes the packing kit YBA-652-2, is part number RYB-921-13 for the 3" valve.
The total rebuild kit for valves sizes 2 1/2"-6" is the same RYB-921-XX prefix where XX is the valve size 12-16
RYB-921-12
RYB-921-13
RYB-921-14
RYB-921-15
RYB-921-16

Please see page 18 and also pages 22-24 of the attached Valve Repair Kit

Schneider Electric Canada

Attachment(s)
Valve Repair Kits F-27688.pdf [8.37 MB]