{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
How can the BMEP58_ECPU_EXT.NETWORK_HEALTH DDT be reset?
Issue
After correcting a network topology or broadcast storm issue on my M580, the Device DDT variable structure (of DDT Data Type = T_BMEP58_ECPU or T_BMEP58_ECPU_EXT) reports that a potential network broadcast storm is detected.

e.g.) BMEP58_ECPU_EXT.NETWORK_HEALTH (Bit 8 starting from 0 in the ETH_STATUS Word)  = 0
which indicates that a potential network broadcast storm is detected.
The value is not reset back to 1 (which means that a network broadcast storm is not detected)

Product line
EcoStruxure Control Expert, Unity Pro, Modicon M580 PLC

Resolution
Before firmware version 2.80 for M580 PLCs, a power cycle of the CPU was required to reset the bit. From V2.80 forward, the bit will reset itself after the problem is corrected.

A firmware upgrade >=2.80 is recommended to correct the behavior.


If this FAQ did not solve your issue, you can chat with us at chat with us or e-mail us at customer.services@se.com to create a case with our Technical Support Team.

If you are not located in North America, please contact your local Customer Care Center for assistance:
Support | Schneider Electric Global (se.com)

Schneider Electric Canada