{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Can the Ground lug in a DASKGS600 lug kit be bought separately?
Issue:
What is the replacement Grounding lug used in the DASKGS600 lug kit ?

Product Line:
LV Transformer Lugs

Environment:
Maintenance

Cause:
Replacement

Resolution:
The transformer grounding lug supplied in the DASKGS600 lug kit is made by Ilsco as p/n D2175. Since we do not make Ilsco lugs, it is advised to contact them directly for sale.
The lug is capable of landing (4) 3/0-350 kcmil wire Al/Cu. See attached for location of 4 conductor Ground lug.

Schneider Electric Canada

Attachment(s)
Ground lug from DASKG secondary lug kit pic.JPG.jpg [63.75 KB]