{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What oil used in a MA-405 actuator?
Issue:
Is the Oil and replacement gaskets available for the MA-4XX Acuators?

Product Line:
Valves and Actuators

Environment:
Maintenance

Cause:
Replacement

Resolution:
The Oil which is supplied for the Actuators, see attached for Oil specification used with the MA-4XX Actuators .It is sold exclusively to Schneider Electric for the Actuators and cannot be purchased .

When disassembling the Actuator, new gaskets would also be needed, and replacement gaskets were available at one time, but are no longer. Recommendation is replacing the MA-405 actuator with a new one.

Schneider Electric Canada

Attachment(s)
MA-418 Hydraulic Oil Titan 15AW.pdf [178.52 KB]