{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What is the bottom cover plate for a 3SQ58110 transformer?
Issue:
What is the replacement bottom cover for a 3KVA transformer 10A style enclosure ?

Product Line:
LV Resin Encapsulated Transformers

Environment:
Maintenance

Cause:
Replacement

Resolution:
This is a special transformer for the GM Plant in Detroit. The 3KVA , epoxy encapsulated transformer has a 480V/575V dual primary 240V secondary which makes it a special.
The enclosure is the standard 10A style and uses (1) short and (1) large bottom cover plates. The Short cover is p/n 39002-288-06 and the Large cover is p/n 39002-287-06

Schneider Electric Canada