{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What wire sizes can be used on the S33100 terminal block for Powerpact P and R frame Micrologic trip units?
Issue:
Wire size for Powerpact P and R Micrologic trip units

Product Line:
Circuit Breakers

Resolution:
Terminals of S33100 are designed for sizes 22–16 AWG (0.3–1.5 mm2) wire.

Schneider Electric Canada

Explore more
Range:
Category:
Articles that might be helpful Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
Category: