{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What does Unity Error - "The configuration Catalog is not compatible with the current application:" mean?
Issue
The following error appeared (depending on the project's CPU or version number):
"Some objects are missing or their version is incompatible. : The Required CPU reference: < BMEP584040 02.40 > is MISSING!"

Product line
Unity Pro, Control Expert

Resolution
This could mean that the project was created with a newer version of Unity than what is trying to open it and BMEP584040 v2.40 does not exist in the version that is being used.  In this specific example, v12.0 is returning the error because it's M580 CPU version selections will only go as high as v2.30.

The project must be opened using the version that created it (or a newer one) and the CPU reference changed from BMEP584040 2.40 to BMEP584040 2.30.  This is followed by another export or archiving of the file. Unity v12.0, in this example, would be able to open the new file without seeing this specific error.

Alternatively, simply upgrading to the latest version of Control Expert programming software will allow the project to be opened as is.

You could also see this error is you are trying to open the project in the above example using a size S as it does not support the BMEP584040. Take a look at Help->About to be certain of the licensed size and version.


If this FAQ did not solve your issue, you can chat with us at chat with us or e-mail us at customer.services@se.com to create a case with our Technical Support Team.

If you are not located in North America, please contact your local Customer Care Center for assistance:
Support | Schneider Electric Global (se.com)

Schneider Electric Canada