{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

What are the DC coils for LC1D40A-LC1D80A contactors?

Issue:
DC coils for LC1D40A-LC1D80 contactors

Product Line:
TeSys D Contactors and Overload Relays

Environment:
North American Products

Resolution:
TeSys D contactor DC coils references from 40A–80A will be substituted by the TeSys D Green coils.
AC/DC coil + DC low consumption coil (BBE for 24V DC compatible with PLC I/O 500mA). AC
coil, such as P7, and TeSys D coils below 38A are not affected.
Exceptions include:
•   Coil JD/JW 12VDC
•   Voltage above 250V, such as RD 440VDC
•   Spring terminals-Ex: LC1D65A3
•   37kW applications-LC1D80A only replace part of LC1D80

Schneider Electric Canada