{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Can the Powerpact B frame breakers be backfed ?
Issue:
Are there Line and load markings on the Powerpact B frame breaker to prevent it from being reverse fed?

Product:
Powerpact B frame Breakers

Environment:
Application

Cause:
Product Features

Resolution:
The Powerpact B frame breaker can be reversed fed , or back fed . It has no markings that would restrict it from being wired in a backfed manner.

Schneider Electric Canada

Attachment(s)
B catalog 0611CT1603.pdf [13.93 MB]