{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What is the AIC rating for the H and J breakers used for Model 4 MCC Feeder breaker buckets ?
Issue:
What breakers are used for 15A-150A and 200A-250A Model 4 MCC feeder breaker buckets

Product:
Model 4 MCC

Environment:
Application

Cause:
Product Features

Resolution:
The Mdl 4 Motor Control Center feeder breaker buckets for 15A-250A, use the HJ and JJ thermal magnetic breakers with a 65KAIC @ 480V provided.

Schneider Electric Canada