{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Looking for a WILPA 1360 battery replacement
Issue
Looking to purchase a WILPA 1360 battery assembly from Schneider Electric.

Product line
Modicon Quantum

Resolution
The Schneider ordering part number for the WILPA 1360 which is a repackaged BR2-3A with a set of leads and AMP #173977-2 plug in connector is 990XCP98000.

All Quantum based controllers use a lithium 3v battery with leads and connector. The Schneider Electric ordering part number for all is 990XCP98000.

There are multiple manufacturers for this type of lithium battery. Schneider used either a BR2-3A, DL2-3A, CR123A or BR17335 lithium 3v battery for this assembly. This battery assembly has also been repackaged with a part number showing either WILPA 1607, WILPA 1608 or WILPA 1949B.

Schneider Electric Canada