{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

What makes the MK2-7121-126 Actuator so special ?

Issue:
Why is the MK2-7XXX Series Actuators obsolete?

Product:
Valves and Actuators

Environment:
Maintenance

Cause:
Replacement

Resolution:
The 2 in the MK2 p/n means it has a High Temp Diaphragm, which is no longer.   The -126 means it has different fittings.   A standard temp diaphragm  MK-7121 actuator can be used with a KEL-B-571 fitting will work for a substitute noting the absence of the high temp diaphragm

Schneider Electric Canada