{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What are the differences between HCJ and HCM interiors?

Article available in these languages: Spanish

Issue:
Differences on the HCJ and HCM I-Line interiors

Product Line:
I-Line

Environment:
Panelboards

Resolution:
The HCJ is an update provided for the HCM Interior frame. Listed below are the updates we have on HCJ I-Line Interiors:

1. All deadfront openings on HCJ interiors are enlarged/widened to allow acces on electronic trip units of Powerpact H/J/L Frame breakers that use Micrologic 3/5/6 trip units.
2. While the width of HCJ and HCM interiors and enclosures are the same, the options for HCJ enclosures are limited to 3 options (48", 73" and 91" high).The 64" option was removed to provide more uniformity in the selection of boxes.
3. HCJ enclosures are 9.5" deep compared while HCM enclosures are all 8" deep. This is to standardize the depth to other I-Line Panelboards and all options in HCJ interiors.
4. HCJ Nema 3R and SS Enclosures are all 9.5" deep to conform with the update on number 3.
5. MLO and Main Breaker options for HCJ begin with 400A instead of the HCM's 225A.

Schneider Electric Canada