Issue:
What is the part number for the traverse spacer kit and connector bar kit noted in bulletins 48049-450-02 and 48041-092-02?
Product Line:
Circuit Breakers
Resolution:
The part number for this kit is SECONKMPNW and is available to Services only.
See first bulletin attached. The other two are older and are provided only for reference.
What is the part number for the traverse spacer kit and connector bar kit noted in bulletins 48049-450-02 and 48041-092-02?
Product Line:
Circuit Breakers
Resolution:
The part number for this kit is SECONKMPNW and is available to Services only.
See first bulletin attached. The other two are older and are provided only for reference.