{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

How can you turn ERMS Maintenance Mode OFF on an MTZ breaker if turned on via a switch, but the switch is not installed?

Issue:
How to turn ERMS to OFF without a switch.  How to disabe ERMS on Masterpact MTZ with ESM Module installed.  This procedure may be helpful when removing the breaker from the cell for primary or secondary injection testing.  See attachments.

Product Line:
Circuit Breakers

Resolution:
  1. Apply 24 Vdc to ESM terminals 484/471 to disengage ERMS (otherwise it will stay engaged even when step 2 is done)
  2. Using EPC, go into accessory declarations and turn off ESM. (Un-declare the ESM in the control unit)

This process will disable the ERMS function in the control unit.

See attachment for ESM wiring diagram and detailed wiring instructions.

Schneider Electric Canada

Attachment(s)

ESM Switch  Module.docxESM Switch Module.docx [143.83 KB]
MTZ Disabling ERMS on MTZ with ESM module installed.docxMTZ Disabling ERMS on MTZ with ESM module installed.docx [1.37 MB]
Explore more
Category:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Category: