{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What parts are needed to have an MTZ2 breaker be electronically operated with communications?
Issue:
Accessories needed for communications

Product Line:
Air Circuit Breakers

Resolution:
Each breaker will need an isolation module, shunt trip, shunt close, spring charging motor, and remote reset (optional). For 110/130 Vac control voltage, the following are the part numbers:

Isolation module = LV850056SP
Shunt trip = LV833035SP and LV847849SP
Shunt close = LV833035SP and LV847849SP
Spring charging motor = LV847893SP and LV847849SP
Remote reset = LV848202SP and LV847849SP

Schneider Electric Canada